Showing results for 
Search instead for 
Did you mean: 

New infographic on generative design

Siemens Genius Siemens Genius
Siemens Genius

gen design infographic.jpg

We have been working with Design World magazine on a new infographic that illustrates some of the key characteristics and benefits of generative design - you can download the full infographic in PDF format at the bottom of this blog post.

The new infographic contrasts the traditional process of using 3D CAD software to turn your idea for a component or product into a detailed design, with the new possibilities that generative design offers. Using the traditional design approach you may need to run through an iterative process where you design the component, apply loads and material to your 3D CAD model, and then run an FEA analysis on the model to see if it performs as needed. For components subjected to significant loads, you may need to run through several iterations of this process to ensure that stress concentrations are reduced and your design has a sufficient safety factor before the yield stress is exceeded.

With generative design, you only need to specify small areas of the final geometry, for example a pivot point where the component will be located and constrained to move in a certain way, a bearing surface where a load will be applied, and any keep-out areas. Generative design then uses computing power and topology optimization techniques to come up with an optimized design. FEA analysis is an integral part of the generative design process so this significantly reduces the need to run these analyses yourself.

The infographic also summarizes the many benefits of generative design, including designing lighter components that use less material, that are suitable for additive manufacturing, and that eliminate additional manufacturing operations like assembly and welding. This infographic is referenced in a more comprehensive article on generative design and an associated competition from Design World. And you can visit our website to find out more about Solid Edge Generative Design.

The infographic contrasts the multiple, designer led iterations of a traditional design process, with faster computer based iterations using generative designThe infographic contrasts the multiple, designer led iterations of a traditional design process, with faster computer based iterations using generative design

Valued Contributor

Is it meant to look like it was put together by a 12 year old kid in MS paint?  No offence meant but it's clunky and very 'South Park'.  I like what you're trying to do but I think it could be done a lot better.



Siemens Genius

 Hello Guy. Thanks for your viewpoint on the infographic that was created by Design World as part of a set of materials to promote a competition that we are running called "Generate Ideas". I believe it has a deliberately simple appearance as the idea of inforgraphics is to present information quickly and clearly. At the same time we will take your feedback onboard for future exercises like this.

Please consider entering the competition, we look forward to seeing your entry!


Valued Contributor

 Smiley LOL I guess I deserved that.  I didn't mean to be overly negative, I just think a 'pro' (certainly not me) could have come up with something a bit better.  I liked the article BTW.