Cancel
Showing results for 
Search instead for 
Did you mean: 

SEU14 video: Creating Blended Surfaces

MLombard
Retired

Here is another presentation that I gave at Solid Edge University this year. This one goes through the surfacing features of a bottle and a bobsled type shape to show how to create a smooth shape when using multiple features.I'm walking through the features showing the folks at the presentation the features and the thought process used in modeling the shapes.

 

Again seeing myself on video is kind of embarassing. Audio on all of these is kind of sketchy, mainly because of the microphone mounted on presenter's shirts.