Cancel
Showing results for 
Search instead for 
Did you mean: 

SEU14 video: Smart Features on Dumb Parts

MLombard
Retired

If you work with imported data from any source, Solid Edge Synchronous Technology is the tool you need to be using. In this Solid Edge University presentation, Chris Dayton of the Solid Edge planning team lays out the capabilities of feature recognition capabilities of the software. "Dumb" parts are a lot less "dumb" in Solid Edge than in other modelers. 

 

Comments
Phenom

This is a good overview of Feature Recognition. I would highly recommend that SE move the functionality into the import/open function instead of buring the recognition inside the pulldown menus. This fits the actual workflow process better.