Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Mobile Viewer now for All Android (4.0 and up)

MLombard
Retired

When thScreenshot_2013-09-26-10-41-32.pnge Solid Edge Mobile Viewer for Android was first released, it was only intended for Android tablets. A discussion on the Solid Edge Community Forum (now into its 6th page) turned into a demand from users for something they could use on their phones. “The best device is the one you actually have with you.” And who carries tablets around at work?

 

It didn’t take long to make a few simple changes, get a few beta users together, test it out, and get it back out on the Google Play Store as something we all could use. So if you have an Android with 4.0 or later, this free app should run on your phone.

 

In case you’re skeptical about how useful a CAD viewer is on a phone, first, it is extremely fast. You won’t believe you’re not on your wScreenshot_2013-09-26-10-03-03.pngorkstation, it’s that fast, at least on my year old Moto Razr HD maxx. Second, it uses a special file format (*.sev) in which you can output parts and assemblies from Solid Edge ST5. For draft documents, you have ST6 MP1. Use the Save As > Save For Tablet command. And third, it’s just cool to be able to rotate and zoom nice looking 3D CAD models on a device that fits in your pocket. I mean, these things have all this power, it’s nice to finally have something that makes use of some of it (other than games).

 

To address some of the negative comments in the reviews, it sounds like people don’t understand that you need the special format file for the viewer. Also, to open the files, you can either put them in your Download folder and they will show up with the samples, or you can just open the file from email or Dropbox and the Solid Edge Mobile Viewer will come up automatically.

It’s a great little tool that I’ll always carry with me, even if I don’t have my laptop. Thanks to Dan, Laura, and the gang for this! I know the guys on the forum are happy.

Comments
Phenom

Keep it up! I signed up for the Beta to get access to this on my Samsung Galaxy S4. Being able to whip out the phone and show a customer their product as we stood on-site was incredible. And we won the job! 

Gears Esteemed Contributor

I would also add....as in most export file types, be sure to check out the options button for the tweaks available.

[as Matt points out....you must have ST6 Maintenance Pack 1 (or later) to be able to export draft files to the viewer]

 

SE_ST6_MP1_DraftExportToViewer_Options.jpg

Gears Phenom

Hi Matt,

 

Thank you for sharing this is a very good article.

 

I've tested it and it works well on my basic LG cell phone.

 

BR,

Imi