Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge ST9 Interface Enhancements

MLombard
Retired

ST9 has some new interface look and functionality. The part I like best is the tabbed design.

st9i1.png

st9i2.png

In this screen grab you can see three tabs for open documents right below the ribbon. You can already access open docs easily by using Ctrl-Tab, but that just goes through the list in a specific order. Using the tabs, you can select them out of order, and visualize which documents are open at any time.

 

Also, you can right click on the tabs and access even more controls for opening or closing windows.

 

You can also right click on the blank area next to the tabs to control the tabs like windows. This is for people who preferred the old window-based way of managing open documents.

 

st9i3.png

On the right end of the tab area is a familiar X to enable you to close the current window/tab, and also a left and right arrow. These are for when there is an overflow of tabs that cannot all be shown on the screen at the same time, allowing you access to the hidden tabs.

 

st9i4.png

Ribbon Color

 

st9i5.png

Also with these screen captures, you can see that the ribbon background has changed a little. You can adjust this by going to the Application Menu > Settings > Options > Helpers > General > Application color scheme. The options are Light Gray, Dark Gray, Black, and White. The default is White, but I personally prefer the Dark Gray (shown below) because it uses color to distinguish between different areas of the interface.

st9i6.png

 

High-resolution Monitors

 

Another bit of UI interface that you may or may not see, depending on your equipment is the support for high resolution monitors. You may remember that in my initial review of the Microsoft Surface Book, there st9i7.pngwas some discussion about how tiny the icons and general interface become at 3000x2000 pixels. These settings in the Solid Edge Options > Helpers allow you to adjust the interface for your combination of resolution and eyesight. These features work with Windows 10, so you may need an OS upgrade to get the full effect of these improvements.

 

This adjustment will also account for gesture size.

 

Application Menu

 

The Solid Edge Application Menu now uses the “Backstage UI”, just like Microsoft Office 2013.

The new interface reflects the growing amount of information that you can access within the Application Menu, and offers an expanded list to help you sort out what you are looking for more easily.

st9i8.png

As a part of the Application Menu, you might also have a look at some of the areas such as the Learn page. This helps organize the various areas for help and support (including the community and certification!)

 

Icons

st9i9.png

 

You will see some new, attractive icons for Solid Edge documents. These will show up when you are not getting thumbnails in Windows Explorer.

You can cycle through the avialable icon sizes by using Ctrl-Scroll Wheel when in a Windows Explorer folder with Solid Edge documents (also works with other document types).

 

Style Palette

 

The Style Palette enables you to select colors for parts in assemblies very quickly and easily. This is a big improvement for anyone who messes with colors. I know a lot of people don’t but they might now because it is so much easier.


The Style Palette is the grid of colored circles in the Assembly Pathfinder area. Just activate it, and drag a color onto it. The color is applied at the assembly level, and in the case where more than one occurrence is in the assembly, Solid Edge will prompt you to select this occurrence or every occurrence.

st9i10.png

st9i11.png

The color is not applied to the part when you open the part in it’s own window. You still have to use the Part Painter for that. Part Painter has also received some enhancements with small preview swatches used wherever only color names used to be displayed.

 

The Style Palette looks and works like the same tool in KeyShot, and because it works in the assembly, it was probably intended to get properly colored models in to rendering quickly so you don’t have to do it in KeyShot. Whatever the reason, it’s a great tool, and will be a big time saver for people who color their models.

 

Last Command Used

 

st9i12.png

st9i13.png

When you use a command from a drop down list, it is sometimes useful for the interface to remember the last command that you used in that list, and put that one at the top. ST9 now allows this. In the image to the right, the original command was Tangent arc, but then you used the Arc By Center Point, and now that command is on the top. This behavior is now controlled via Application Menu > Settings > Options > Helpers > Command > Last Used Command (in droplists) Stays On Top.

 

Summary

 

There are a few new things to get used to here. Nothing really earth-shattering on its own, but all of this is definitely useful, and helps keep Solid Edge in line with industry interface standards. Interface enhancements are always a little disruptive because they take some time to learn, but the improved productivity is worth it. Especially in the case of theTabbed interface, Style Palette and the Last Used Command.

 

 

Comments
Genius
Genius

Tabs and Last Command are definitely welcome!

Gears Esteemed Contributor

Last command used - stays on top.......hallelujah!

 

I've been using a registry mod to achieve this, but it is session specific, and restores to defaults after restarting SE.

Please let that not the case in this enhancement. [say's that, every so hopefulRobot wink

 

 

Excited to get my hands on ST9.....soon.

Phenom

Matt-

Great to see that the interface is following the MS Office layouts. People may or may not like that but the consistency makes for easier discoverable functions and that means easier to learn!

 

I'm also glad to see high resolution functions included. Although, Windows 10 has been generally accepted- even by the DoD- I believe most companies are still running Win 7.

 

I'm not sold on the tabbed window functions. To me, it's just something taking up graphic real estate. I'd have to work on it to understand how it benefits the user. (I like to work in-context of the assembly.)

 

Finally, it is nice to see that the dreaded blue/gray monochromatic color scheme was NOT used! Meaning there is a good use of color contrast. If this statement doesn't ring a bell, just see what others are saying about their other CAD systems user interface! It ain't pretty and they ain't happy at all! 

Builder

     I have to chime in on this. I work in a retail fixture company that manufactures wood cabinets, glass showcases, slatwall etc....with the majority of our work being particle board/mdf/plywood finished in a laminate or melamine or solid surface material and color is VERY important. I switch colors often, clients want to see different cabinets in different colors "lets say yesterday".

     I have noticed this color palette in ST9 and after tinkering with this a bit.....have sort of a negative feeling towards this "style palette".........and reason being is I see that the potential is there but in then end you still have to go into each part and apply your desired color again to each face/part. For me theres no reason for me to have to apply a color twice, since in the end you still need to apply the color in the part environment.

     Now you can move a hole in sync and it save to the part level. And now you can apply a color at the assembly level to a part but it will not save to the part level Smiley Sad I think if this "New" style palette had the option to let you choose face/body/feature/any and then save to the part level........THIS WOULD BE AS INNOVATIVE AS SYNCHRONOUS TECHNOLOGY.......or almost. I would probly be 50% more effecient as well lol.

     Hopefully a developer will see this recommendation!!!!!!