Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Tips and Tricks #10

MLombard
Retired

1) How do I insert grounded parts at the origin of an assembly file?
The first part inserted into a new assembly is by default grounded and placed at the origin. To place other grounded parts into an existing assembly at the origin of the file, you can use two methods:
1. Go to the Part Library tab and while holding the CTRL key, double click the part file. This will place and ground the part at the origin.

2. In a Windows Explorer window, right click and copy the part you want to place. In Solid Edge go to the Home Tab. While holding the SHIFT key, click the PASTE button located in the Clipboard group. This will place and ground the part at the origin.
 
2) What determines the Author name in File Properties>Summary?
Your Windows username will be the Author name when you create a new file. It can be manually overwritten.

3) Where can I find instructions for setting up Standard Parts?
Once you’ve installed the Standard Parts Administrator, the User Guide will be in the Start Menu under All Programs -> Solid Edge ST7 -> Standard Parts.

4) How can I scale geometry in draft?
You will have to use the scale command that is located under the move command. Follow the prompts at lower left and geometry will be scaled.

5) The drawing view shows the complete assembly but the parts list only shows a few parts?
Typical causes for this behavior include using a display configuration in the view or parts list, or the parts being turned off form showing up in reports in via Occurrence Properties in Assembly.
 
6) How do you open a .SEV file?
This is a mobile app viewer file which can be opened with the Free Solid Edge Viewer App available for Android and IOS devices.

7) How can I get the measure commands to be active in the free viewer?
The free viewer does not have the measurement commands in it. An upgrade to view and markup will be needed.

8) How can I remove a part copy link when parent link is broken?
You can move part copy from the ordered environment to the Synchronous environment and then Solid Edge will remove the part copy link from the file.

9) How can I Update an existing KeyShot assembly rendering after adding more parts to assembly?
You will have to have the original .bip file open in KeyShot; then in Solid Edge assembly hit the render button a message will then pop up stating there is already a rendering of this file do you wish to use the file and update it to match current assembly view. You will then hit ok and in KeyShot the view will update in the open .bip file.
 

Comments
Community Manager

In case you are wondering where/how Matt decides on these tips/tricks -- which I must admit seem rather random -- these are actualy questions that come into the GTAC team in HSV. They answer user questions and then write it down at the end of the week to capture it for the future. That is why this seems so random -- and it is in a good way -- just a slice of life for GTAC!

Gears Honored Contributor
Phenom

Dan thanks for giving everyone insight as to where these topics arise. Now that we all know the origin of these, is there a formal method of requesting one, or is it simply based on Development's sense that there's a need for greater clarity?

 

I think Matt and SE Development should be applauded for being so responsive to the community... and maybe should take more credit by mentioning that this was based on another User Question. This would show ALL users especially the newbies how great the Solid edge community is, but more importantly how truly great Solid Edge Development is at listening to the users.

 

Again thanks for shedding light on this.

 

Bob