Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Tips and Tricks #7

MLombard
Retired

Is there a way to find out what all of the two-letter codes are for callouts?

 

tipsandtricks4.pngYes. Go to the Callout command and select the Property Text button from the Callout Properties dialog. Now click on the “Symbols and Values” button down near the bottom of the Property Text dialog. This will bring up a third dialog which has all of the two-letter codes sorted into groups. Expand the grouping tree to find the codes you might be looking for.

 

 

Can I create a user-defined material with its own density?

 

solidedgetips6.pngYes, you can create a new material in the Solid Edge Material Table (Application menu> Properties> Material Table) and assign user-defined properties and values to it. To add a material, right click on the material family folder (such as Steel, Iron, etc.) and select New Material from the list. You can also copy an existing material from the list and paste it into the folder. Make sure to give it a new name when you do this, and also make sure to change the appropriate individual properties.  These properties will then be assigned to the part once they are applied to the model.

 

 

Why am I unable to rotate a Section View pulled from a broken view?

 

There are a few factors which play into the ability to rotate a view. First, the view must be unaligned from the view from which it was pulled. Second, you must undo the “Show broken view” button. Finally, the break lines must be deleted from the view. After this, the Section View will rotate. After the rotation, you can recreate the break lines.

 

 

How can I change the edge color of a part in a drawing view?

 

Right mouse click on the Drawing View, select Properties, click on the Display tab, select the part, and select a visible edge style which has been configured with the desired color.

solidedgetips7.png

 

How to hide individual edges in a drawing view?

 

solidedgetips8.pngDrawing View edges can be individually hidden by the Hide Edges command. The command is located in the Ribbon, on the Home tab, Edges group. Just click the edges to be removed from the drawing and they will not be displayed anymore.

 

 

Why does selecting “Use Designed Assembly” only toggle the first level?

 

Prior to ST7, if you selected “Use Designed Assembly” all subassemblies that were simplified would be toggled to designed, no matter how many levels there were. In ST7 only the first level subassembly will be affected. If you want to toggle all levels you can press and hold the [CTRL] key while selecting the “Use Designed Assembly” command.

 

 

Why can’t I select a region for the cross section curve in ST6 in a synchronous helical cutout command?

 

You have to select each edge of the closed cross section individually AND also the axis in one single step to make this work. Improved in ST7 by letting you select a region for cross section and axis in two separate steps.

 

 

Why am I seeing my thread feature in a front view but not in the right view of the assembly drawing?

 

 

solidedgetips9.pngThe problem seemed to be because of the default tolerance setting for "thread axis tolerance". But we were able to override this and use a value of .01 deg. After this when we updated the view the thread showed up on the right view. You can find this setting in "Drawing View Properties/Advanced tab". Update the view after overriding the default tolerance.

 

 

What are the advantages of dropping flow lines and having annotation flow lines?

 

solidedgetips10.pngAnnotation flow lines have the full range of edit. They are not used for exploded animations, but are designed for making drawings. You can draw and modify them to get what is needed in the drawing view. Drop is only available in ERA (on the Tools tab), which is only available in assemblies.

Comments
Gears Esteemed Contributor

I have a question about the users "New Materials"......can we rearrange the order of the list? Currently, all new entries go to the bottom, but would be MUCH BETTER if they could be moved to become grouped with the other similar entries.

 

ST7_Material Table.png

Phenom

 

@SeanCresswell   I opened an IR becasue of this... Our list is out of order in ST7 where it was ordered in ST6, (alphabetical sort a-z)  This is currently works as designed but converted to an ER.

 

Export to Excel - sort in excel - Re-Import.

 

Snippet From IR Resolution Letter.

 

"Sorting is currently not supported in the material table. For now the workaround is to export the material table in Excel, sort the materials in excel and again import the material table. But this can be time consuming and prone to errors. So we need to support sorting and should be applicable to Library, Directory, and Materials. We are coverting this to an ER so a project can be defined and implemented in a future version. "

 

ER is #  7323866  is folks want to join

Retired

Thanks for following up, guys!

Phenom
Phenom

I had from a long time difficulties with some lines that exists but I wasn't able to make them visible in the Draft.


But changing the value of the VHL-Tolerance from Standard to 2 makes a big difference!


Regards,


YasserSE_VHL_Tolerance.jpg

SE_VHL_Tolerance.jpg

Retired

Whoa!YD, thanks for that, especially the visual comparison. That's important to know!