Cancel
Showing results for 
Search instead for 
Did you mean: 

Standard Parts- Installation of Standard Parts Administrator.

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Fasteners are an integral part of an assembly; they are used to affix two or more parts together. The following information will help novice users to understand the installation and administration of the Standard Parts functionality in Solid Edge.

 

Typical workflow to install Standard Parts

  1. Install Solid Edge
    • Solid Edge installation is pre-requisite for Standard Part Administrator Installation. 
      • Standard Part admin will not install without Solid Edge on system.
  2. Install Standard Part Administrator (SPA)
  3. Install Machinery Library
  4. Install Piping Library

Installation of Standard Parts Administrator

Solid Edge Standard Parts is a robust administration system that allows designers to use fasteners, bearings, structural shapes, pipes, fittings, etc. – quickly and efficiently. Models showing this level of detail make it easier to create complete bills of materials, get assembly weight and center of gravity, show more realistic pictorial views and renderings, as well as assist in the creation of assembly or maintenance instructions.

 

There are two major workflows of standard parts

  1. Standard Parts for single user
  2. Standard Parts for multiple users (network installation)

Standard Parts Administrator installation for Single User

  1. For single user SPA can be installed on C:\Solid Edge Standard Parts or any other location

Standard Parts Administrator installation for multiple users

  1. Install the standard parts on shared UNC location.
  2. Install the Management Studio to create the external database
  3. Configure the working database to external data base
    • Create external network database using database manager

Tech Tip to install Standard Parts Administrator for multiple user

Here we will discuss some tips to install Standard Parts Administrator.

  1. Best practices to Install Standard Part Administrator
    • If SQL is not detected on system, set up will start SQL Express Installation as part of Standard Part Administrator.
    • Create share where you want to install Solid Edge Standard Parts.

 1.png

 

Note this path in UNC format

  1. \\<Machine Name>\<Shared Folder Name>2.png

 Run the Standard Parts Administrator setup exe

             3.png

 

Once you run Standard Parts Administrator set up exe, you will see below dialog

4.png

 

Click on Next

5.png

 

Click on Next

6.png

 

Select ‘This feature and all subfeatures, will be installed on local hard drive’

 

7.png

Click on Next and set the folder

 

 9.png

 

Click on Next

10.png

Click on Install

8.png

 

 Start installing Standard Parts Administrator

 11.png

 

Click on Finish to complete the installation

12.png

Once you scussefully install the standard parts SAC file will be seen on Solid Edge Options dialog under File Location.

 

To set the 'External network database' Click on 'Configuration Wizard'

 

13.png

 

 

Open configuration wizard and click on 'Browse'

 

 

14.png

 

Select 'External network database' from 'Database Manager'

15.png

 

Start Solid Edge on machine, start a new assembly. From Solid Edge Options-File Locations

 

16.png

 

After completing these steps, Standard Parts is ready to use with the free sample standard parts content. If you want to use the full content of Standard Parts libraries then you need to install Parts Libraries.

Comments
Solution Partner Pioneer

Excellent.

 

I have one problem from "Select 'External network database' from 'Database Manager' ".

 

I can't create 'External network database'.

 

I am select 'External network database'  & give user & password, Database Manager take both correct and then after Deselect 'External network database' option and  reselect 'Local Database'.

 

Please do needful.

 

Thanks & Regards,

Irfan Pathan

Dreamer

 Dear  

 

After Install SolidEdge ST 09 and continue to install Standard Part Administrator and Machinery Library, I still cannot find Bearing, Circlip, O-Ring and Power Transmission like Gear and etc.

 

Need help and Solution

 

Regards

 

Iskandar

Solution Partner Pioneer

Exellent.

 

One thing that is very important for Standard part with Server base installation.

 

Go to "Sql ServerConfiguration Manager" & See imagae for more details.

 

SE_Standard_Part_Sql Configuration.pngSet port 1433 when standard part configuration wizard not set serverbase database