Cancel
Showing results for 
Search instead for 
Did you mean: 

The Community at SEU14

MLombard
Retired

IMAG0234.pngAs soon as it’s started, it’s all wrapped up. I have to start by thanking all of you that read this blog. Several people came up to me during the event and thanked me for writing, just letting me know that the effort going into this is appreciated. Thanks to all the readers – those who leave comments, and those who just lurk. A blog is nothing without readers.

 

Now that SEU is behind us, I can stop pleading with you to come, and start telling you about what you could have learned had you been there. Since Dan showed ST7 publicly, and we have the web page up (you gotta check out this website if you’re interested in ST7), I can write about IMAG0242.pngthe new features more freely here. Like last year, I’ll also go through some of the presentations from the event and comment or highlight various items that I think are interesting. I may invite the presentation authors to join me in discussing the topics as well. There are tons of things we can do to make the technical stuff both informative and interesting.

 

Certification. Yes. It happened. There were two certification sessions at SEU14. A fair number of folks took the tests. There is no official word on who will be our first certified users, but the news will come out shortly. This is the ground floor of a program that is going to grow. You’re eventually going to want to be part of this. The initial test was fairly low tech, but the process will develop into a modernized system that is accessible and valuable to professionals, employers, students, and educators.

 

Yes, I took the test. While I’m certain I didn’t pass, I will set it as a goal to pass it within the next year. I really felt like I needed to know what the test was all about, so I took it even though I knew I wasn’t really ready for it. I don’t think I have too far to go to be able to pass it. I need to gain some credibility here with some Solid Edge chops.

 

original.pngDownUnder Blunder. Rick Mason put together a great contest. In the end, no one actually finished in the time allotted, but from the results, it looked like at least one person was very close. The winners were

 

#1: Daniel Rubio

#2 : Cody Hunter

#3: Wayne Ward

 

Thanks again to Rick Mason for putting together this year’s contest. Stratasys printed out the models as trophies for the winners.

 

medium.pngCommunity awards. Karsten Newbury gave out community awards at the end of the event to several people who have really helped the community to grow. I need to call these people out publicly and thank them for their efforts. Some of the awardees were not in attendance, but the four in the photo to the right were.

 

Ken Grundey

Sean Cresswell

Luc Poulin (on stage)

Kyle Joiner (on stage)

Bob Henry

Tushar Suradkar

Larry King

Bob Mileti (on stage)

Imre Szucs

Dylan Gondyke

Jason Newell (on stage)

Marcio Silva

 

Of course making a list is a terrible thing to do if you make a mistake and leave someone off of it, and I’m sorry if I’ve done that. I did exclude reseller partner employers. Imre Szucs was not mentioned on the main stage because he works for a reseller, but after having a couple of conversations with him here in Atlanta, he has definitely earned his place on this list. Jason Newell is also a partner of sorts, but he has also put in an immense amount of his own time, effort, and saint-like patience to make things happen on the developer side of things that would have simply never happened without him.

 

Guys like Ken Grundey and Sean Cresswell are answering questions daily. Without this sort of dedication, this place would quickly fade into irrelevance.

 

Tushar Suradkar is a more recent rising star in the community, but his efforts in the forum and especially on the blog have made a direct impact on our members.

 

Not only do the people who answer questions deserve a lot of credit, but there would be nothing to answer if there were not community members who ask questions. So “thank you” to those of you posting questions. For everyone who asks a question, there are 10 people lurking, wondering the same thing. So don’t be shy. The great thing about a forum that reaches a lot of people is that someone knows the answer to your question.

 

IMAG0250.pngThe live Solid Edge University event is over for this year, for we can get much of the benefit of coming together from this online community. Thanks to everyone who helps make it a useful and even fun destination for all things Solid Edge.

Comments
Gears Esteemed Contributor

Thanks for the recognition. I really want to be at the next event....and am working on it. Although, the online merchandise store will be taking from this budget. Robot Very Happy

Gears Honored Contributor

Matt,

 

Recognition is the ultimate reward for a contributor.

Thanks for your words of appreciation, this really helps me keep going.

 

Once online and logged into the community, it is stalwarts like Ken Grundey, Sean Cresswell, Bob Mileti, Martin Bernhard and Imi who inspire to start tapping at the keyboard and answer questions posted on the forum.

 

Jason Newell deserves a big mention for he is the sole lighthouse for the programming community.

Enthusiast
Sean
 
For next year, remove the hotel from your budget, since I plan to be there I can share the room and no need to split.
 
As for the event cost, I'm sure you can find a way to present one or two session so this can as well be removed from your budget.
 
The only thing left is to find a taxi cab with good wipers :-)
Gears Phenom

My friend Matt,

 

Thank you for your kindly words. The "backstage" is enough good for me... Smiley Wink I'd like to see 2x-3x more names (instead of mine) in the future and I'll be happier because SE community is getting stronger!

 

C'mon Solid Edge!