What’s New in ST10: Data Management

MLombard
Retired

The Solid Edge built-in data management tools added in ST9 are already being enhanced! Here are some of the non-Teamcenter changes for ST10. solid-edge-whats-new-st10-data-management-1.png

 

1) There is now an option to turn Solid Edge data management on or off. If it is off, you don’t have to worry about any of the settings, so they disappear. When it is on, all of the data management options become available.

2) ST10 includes a new Revisions command on the Data Management tab. You can use this to access the entire history for a particular document if you have an established Solid Edge vault. The vault is set up in the Solid Edge Options > Manage > Vault Definition tab.

You can add revisions or make any existing revision the current revision. If you have an assembly open with a part for which you change the current revision, Solid Edge will replace the part in the assembly to match the current revision. solid-edge-whats-new-st10-data-management-2.png

 

Vault setup basically entails directing the fast search to particular folders in a vault definition text file. This portion is not new in ST10, and more detailed information is included in the Solid Edge Help file.

 

3) The Get Latest command, also on the Data Management tab will solid-edge-whats-new-st10-data-management-3.pnghelp you find parts in the active assembly that are not the latest revision, and a newer revision is available.

This ability to replace parts with newer revisions in this level of simple data management is really great functionality, and extremely useful in some situations. You may not appreciate this until you’re in a revision bind and need the tools in a panic.

4) Automatic File Naming is something I saw mentioned in the forum recently as not being in the software yet. Well, here it is. Solid Edge has long had the document name formula to help you build file names from various component properties, but now Solid Edge data management will automatically name files using the Document Number and Revision properties. You can access the options for this functionality in Solid Edge Options > Manage > Document Naming Rule tab, as shown below. This helps you find and/or avoid duplicate file names, which is the reason it requires you to have a vault defined. Solid Edge will search within the vault to make sure no duplicates exist. [Note: Data management without a database is generally intended for those installations where there is no IT or dedicated admin resource available who understands how to administer database applications. It is also generally intended for smaller installations. If you have some question about what method is most appropriate for your organization, I would suggest work with your reseller to match your needs with the appropriate software tools.] solid-edge-whats-new-st10-data-management-4.png

 

 

 

solid-edge-whats-new-st10-data-management-5.png

 

5) Open Drawing is another new command on the Data Management tab. It will automatically find the drawing for the currently active document so you don’t have to do a Where Used search to find it. You can also access this command via RMB in the PathFinder to open a drawing without the need to open the part first. This is a nice touch.

6) Recognition of Standard Parts Design Manager will identify parts from the Standard Parts library so that they are not duplicated or revised or moved to the vault. Again, this functionality is only available to vault users. Go ahead and set up that vault if you haven’t done it already.

Comments
Genius

Vault setup basically entails directing the fast search to particular folders in a vault definition text file. This portion is not new in ST10, and more detailed information is included in the Solid Edge Help file.

 

I took a look at the help in ST9 and there is no mention of vault at all. The only option in SE that I could find is:-

 

  1. Custom Properties
  2. Set Locations (Goes to Windows indexing feature)

 

2017-06-25_13h54_18.png

 

While I am here there is a couple of questions on Data Management that I would like clarified.

 

  1.  Revision files. When I revise a file I can specify a new location for the newly revised file, but there is no option to change the directory of the old (now out of date) file. Can you explain the logic here please. How does SE expect the file structure to be?
  2. File Locations. There is an option to select where Released and Obsolete files go, but those locations are absolute. Where I (and I am sure others to) keep specific files to either a job specific folder or Client/Job specific folder. For example Clients>Client1>Job1>Models any out of date or old revisions would go to Clients>Client1>Job1>Models>Obsolete folder. A relative not absolute file reference. Can this be achieved?

    2017-06-25_14h09_45.png
  3. File Types. In the image above there are Pre-Released, Released and Obsolete file types and their paths. However in Design Manager the options are In Review, Obsolete and Baseline. How do these relate as Obsolete is the only match.
    2017-06-25_14h10_00.png
  4. I see in your blog that there is an option in ST10 to add a prefix to a file name. Does this mean a new assembly, part and  sheetmetal template needs to be created for each new project so to keep the prefix relative to that particular project? Again does SE expect ALL document numbers for ALL projects to be one continuous numbering system?

 

Sorry for all the questions, I am new to SE and clarification on these points may make it a lot easier to get the most out of the product.

Labels