2D model color

Experimenter
Experimenter

Hello,

 

Is there some fast and easy way to make all the lines, polylines, circles, etc one color using VB.net?

 

So far i have tried looping lines, circles, arcs, bspline curves, ellpises and elliptical arcs with something like this:

 

Dim Line As SolidEdgeFrameworkSupport.Line2d
Dim Lines As SolidEdgeFrameworkSupport.Lines2d


        For i = 1 To Lines.Count
            Line = Lines.Item(i)
            Line.Style.LinearColor = RGB(0, 0, 0)
        Next

 

But looping all these elements is really slow and it still does not cover polylines. What would be a better way to solve this problem?

 

Thanks,

Silver Reinart

4 REPLIES

Re: 2D model color

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You may change the color of all used styles directly and then redraw the view:

Dim NewLineColor As Int32 = RGB(0, 0, 0) ' Black (RGB)
' Change the line style
Dim objDoc As DraftDocument = objApp.ActiveDocument
For Each lineStyle As LinearStyle In objDoc.LinearStyles
    lineStyle.Color = NewLineColor
Next
' Update the drawing window
Dim objWin As SheetWindow = objDoc.Windows.Item(1)
objWin.Update()

BUT: If there is any drawing object with an overwritten line color, you have to change the color for that object in its Style property to overwrite it again, like you were already doing!

Actually, I don't know of any API function to remove the overrides, like is is possible interactively. I believe the RemoveAllSegmentedStyles() on each drawing object does NOT do that, but I haven't checked it yet.

Re: 2D model color

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you really need to change the color individually for each drawing object, than you should disable ScreenUpdating and some other properties on the Application object. This makes the execution much faster:

Dim NewLineColor As Int32 = RGB(0, 0, 0) ' Black (RGB)
' Disable any screen updating and UI updates
objApp.ScreenUpdating = False
objApp.DisplayAlerts = False
objApp.Interactive = False
' Update all drawing objects
Dim objDoc As DraftDocument = objApp.ActiveDocument
For Each lin As Line2d In objDoc.ActiveSheet.Lines2d
  lin.Style.LinearColor = NewLineColor
Next
For Each arc As Arc2d In objDoc.ActiveSheet.Arcs2d
  arc.Style.LinearColor = NewLineColor
Next
For Each cir As Circle2d In objDoc.ActiveSheet.Circles2d
  cir.Style.LinearColor = NewLineColor
Next
'... more to do here (PolyLines are represented as LineStrings)
' Enable again screen updating and UI updates
objApp.Interactive = True
objApp.DisplayAlerts = True
objApp.ScreenUpdating = True
' Refresh the drawing window
Dim objWin As SheetWindow = objDoc.Windows.Item(1)

Re: 2D model color

Experimenter
Experimenter

Disabling ScreenUpdating and other properties made it fast enough for me.

 

But I am still struggling to change all of the objects.

 

lines.png

 

The DXF origins from AutoCAD, the names of the green objects are for example AcDb3dPolyline-A89B. They seem to be polylines, but I can't find polylines under SolidEdgeFrameworkSupport method. What else could it be?

 

Thanks,

Silver Reinart

Re: 2D model color

Tushar 2nd Gear
2nd Gear

Try using Spy for Solid Edge to check what type of Solid Edge Objects they are.

Possibly ComplexStrings.

 

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group