Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

64Bit-Addin

Valued Contributor
Valued Contributor

 

Hi all,

i try to make a 64Bit-Addin using Visual Studio 5 with C# under Windows XP 64, Solid Edge64Bit.

Under Windows XP (32Bit) the Addin works fine, but using 64Bit-SolidEdge it doesn't work.

I think the automatically produced COM-Wrappers (Interop.SolidEdgeAssembly.dll etc...) are corrupt.

Using the Dependency Walker it looks like a 32Bit-Dll refer to 64Bit-Dlls!

 

Any ideas?

Regards

Ralf

 

Posted by: Ralf K
Post date: 6/17/2008 9:54:40 PM

2 REPLIES

RE: 64Bit-Addin

Valued Contributor
Valued Contributor

 

Is there anybody who has written 64Bit-Addin, using ".net"???

Regards

 

Ralf

 

 

 

 

 

Posted by: Ralf K
Post date: 6/19/2008 10:40:08 PM

RE: 64Bit-Addin

Valued Contributor
Valued Contributor

 

Hello,

Are you using the 64bit template in Visual Studio? Is it set to Debug Mode with 64Bit enabled? Are you getting any errors while referencing the 64bit SE assemblies in your solution? If I compile a solution with 64bit, I'm not able to run it at a 32bit machine/OS.

I have no experience with SE & 64 bit, but for sure it will the next big issue...

Sibi

 

 

Posted by: Seb Sosna
Post date: 6/20/2008 11:05:02 PM