Cancel
Showing results for 
Search instead for 
Did you mean: 

API/Program error ? Include states of ModelNodes -> Balloons !! Please confirm!

Valued Contributor
Valued Contributor

Hallo,

 

can anyone confirm this with ST4MP2 (or that itis working in older Version),

we switched rom V19->ST4, now we got this problem with API/SE.

 

We use our own tool to set up the draftlist(include/exclude subasm.-parts) as preperation for the standard SE-GUI (under BOM), which then places the baloons.

 

SO:

 

1. Setting up the include-states of ModelNodes within the .net & API (u can also try it with Jasons EdgeSpy!) like this:

 

ASM (Application\ActiveDocument\ModelLinks\[1]\ModelNodes)

....

+dummyASM inc=false (pos=-1) (ModelNode)

++Part1 inc=true (pos=12)

++Part2 inc=true (pos=13)

+dummyASM .....again same state^^

+anotherdummyASM .... also included subasm

....

+normalASM inc=true (pos=12)

....

 

^^ I'd like Edge to place the Balloons onto the subparts (bigger asm for shure  )

 

2. Calling the BOM dialog with place balloons results in:

* totally exclution of the dummyASM, can be seen in the gui and objects:

 

ASM

+dummy inc=false (pos=-1)

++Part1 inc=false (pos=-1)

++Part2 inc=false (pos=-1)

 

https://skitch.com/sonic81/g1chh/unbenannt

 

it seems to be a SE bug with API/Object model, because setting state over SE-gui works -> baloons and Pos is alright + is persistent in the gui/objects; but if I do change even a single ModelNode with the api, the dummy gets switched into excluded in SE-gui again ;(

 

^^ OR has the method of setting it up changed with STx, by usage of any other object ??

 

Please confirm and ifalso got problems pls make a call, too 

discussion is also on http://bbs.industrysoftware.automat...post215767

THX !

 

Posted by: Linus Hechinger
Post date: 12/18/2011 9:33:22 PM