Cancel
Showing results for 
Search instead for 
Did you mean: 

About SolidEdge CommandID!

Valued Contributor
Valued Contributor

 

Hi, all!

I want to know the SolidEdge CommandID!

I use the "StartCommand"!

How to look for the CommandID!

For example: inspect--MV--Physical properties--Update(button). Please help me look for this  CommandID!

thanks!!!

 

Posted by: fat kids
Post date: 7/26/2009 11:04:19 PM

6 REPLIES

RE: About SolidEdge CommandID!

Valued Contributor
Valued Contributor

Solid Edge Spy has an "Event Spy" option. There you can watch the AfterCommandRun event.

 

Posted by: Jason Newell
Post date: 7/28/2009 4:07:23 PM

RE: About SolidEdge CommandID!

Valued Contributor
Valued Contributor

 

thanks Jason.

I use the "Event SPY" look for some CommandID, but some couldn't find.

For example: inspect--MV--Physical properties--Update.

 

Posted by: fat kids
Post date: 8/9/2009 10:47:17 PM

RE: About SolidEdge CommandID!

Valued Contributor
Valued Contributor

Hi fatkids,

 

the event AfterCommandRun is avaliable only for the popup "Physical properties" and not for Button "Update". I think, the CommandIds are not for all functions avaliable.

 

Regards

jr

 

Posted by: JR
Post date: 8/10/2009 9:51:34 PM

RE: About SolidEdge CommandID!

Valued Contributor
Valued Contributor

 

You are trying to invoke an event on a dialog box. That is not a command in and of itself that you can get to using StartCommand. But here's a trick for obtaining actual command IDs. you can invoke that way:

HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version xxx\ToolbarSettings\TooltipCmdId - add this as a DWORD and set its value to 1 (non-zero should do).

Edge will add the command ID to the tooltip it shows when you are over a toobar button or menu (Pre-ST) or over an entry on the command ribbon (ST).

 

Posted by: R.D. Holland
Post date: 8/14/2009 9:30:15 AM

RE: About SolidEdge CommandID!

Valued Contributor
Valued Contributor

thanks

I learned.

 

Posted by: fat kids
Post date: 8/19/2009 10:10:26 PM

RE: About SolidEdge CommandID!

Valued Contributor
Valued Contributor

Hi, you can find a file named secmdmap.xml in the directory of SE program. You can get you want in this file.

 

Posted by: assassin 007
Post date: 8/25/2009 5:56:49 AM