Cancel
Showing results for 
Search instead for 
Did you mean: 

Add some default tolerance values to the tolerance list

Creator
Creator

Hi All,

I'm working on a drawing automation project in Solid Edge ST9. I want to add some default tolerance values to the upper tolerance and lower tolerance list. When the user tries to add tolerances to any dimensions, this tolerances should be readily available. Please anyone come up with a solution as fast as possible.

 

Solid Edge ST9

VB.NET

 

Thank you

1 REPLY

Re: Add some default tolerance values to the tolerance list

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hi @Admin2,
I think that you talking about the combo boxes in the Userinterface of the Dimension command.
The values are stored in the registry, when the user types a new value.
You find these values here:
HKEY_CURRENT_USER\Software\Unigraphics Solutions\Solid Edge\Version 109\PrefSets\Dimension
The values are UpperTolerance1, 2, 3... or LowerTolerance1,2,3... for alpha tolerances.
I dont know how many values are supported.
For Unit Tolerances I cound only find one value. I have no idea where the other values are strored.
regards

JB
SE ST10