Cancel
Showing results for 
Search instead for 
Did you mean: 

Another debug problem with x64 Addin

Valued Contributor
Valued Contributor

Hi,

I've got another debug-problem with x64 vb.net addin onwin7 x64 system withx64 SeST3 pack7,

the addin loads, but there's something wrong cause i can't attach to the addin for debuggin it,guess VS2010 made something wrong, or was it me ?

If I look in AddIn-Manager at the AddIn Properties in Solidedge the path/name of the dll is:mscoree.dll in C:\Windows\System32  

I registered the addin using:C:\WINDOWS\Microsoft.NET\Framework64\v4.0.30319\RegAsm.exe /codebase "%ProgramFiles%\PathTO\Addn.dll"setting the project output path in VS2010 to the Addin path registered aboveregistered with reg to the environments:[HKEY_CLASSES_ROOT\CLSID\{...}] 

@="Name"

"409"="Name"

"AutoConnect"=dword:00000001

[HKEY_CLASSES_ROOT\CLSID\{...}\Implemented Categories\{26B1D2D1-2B03-11d2-B589-080036E8B802}] 

@="Name"       ......

^^ is this so wrong or what's the problme / fix

THANX

 

Posted by: Linus Hechinger
Post date: 9/22/2011 10:49:54 PM

1 REPLY

RE: Another debug problem with x64 Addin

Valued Contributor
Valued Contributor

Hi,

 

i've the same problem in the same situation...

x64 vb.net addin on

win7 x64 system with

x64 SeST3 pack9,

 

I really can't understand what i miss. I add that the debug works correctly when i call regasm for the registration

Thank you

 

Posted by: Alessandro Gaiarin
Post date: 11/18/2011 9:39:37 PM