Cancel
Showing results for 
Search instead for 
Did you mean: 

Arrays in C#

Valued Contributor
Valued Contributor

Hi,

 

certain methods for SE require an Array as a ref parameter (SolidEdgeGeometry.Vertex.GetPointData for example). In VB.Net I could pass a array of doubles, but in C# I can only pass a System.Array. I realise that I can declare something like:

 

Array a = new double[] { };

 

but then when I use the array after the call I have to use (double)a.GetValue(0) to get the first member of the array. Using reflection is one way of doing this, but with ref parameters it gets really messy, and I have to copy the parameters passed back into my array:

 

byte[] idBytes = new byte[] { };

ParameterModifier refParam = new ParameterModifier(1);

refParam[0] = true;

Object[] args = new Object[] {idBytes};

typeof(Occurrence).InvokeMember("GetReferenceKey",

System.Reflection.BindingFlags.InvokeMethod,

null, occ, args, new ParameterModifier[] { refParam }, null, null);

idBytes = (byte[])args[0];

 

Ugly

 

Is there a better way??

 

Cheers

Calum

 

Posted by: Calum McLellan
Post date: 8/16/2006 8:57:03 PM

1 REPLY

RE: Arrays in C#

Valued Contributor
Valued Contributor

I believe you are correct Calum

 

Posted by: Jason Newell
Post date: 8/21/2006 2:40:30 AM