Assembly Study


Good morning,
i have a little problem to studies a tree's assembly.
By I want to write in a txt's file all component name of my assembly but after differents tests i didn't do this.
Can you help me to resolve this problem?!
Thank you very much and good job




Re: Assembly Study


Hi Francesco,


Could you explain a bit more in detail what you tried already and what didn't work exactly?




Re: Assembly Study


Excuse me for my explanation imprecise.
Now as an assembly can not print the paths of all the top-level components parts or assemblies that are. But if I wanted to capture the information also subassemblies and print the paths of their components ?!

This is the code that I have done so far for printing

    Private Sub Button1_Click (ByVal sender As Object, ByVal e As System.EventArgs) Handles Button1.Click
Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objAssembly As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objRelations3d As SolidEdgeAssembly.Relations3d = Nothing
        Dim obj () As Object
        Dim objOcc As SolidEdgeAssembly.Occurrences
        Dim path (0) As String
            'Connect to a running instance of Solid Edge
            objApplication = Marshal.GetActiveObject ("SolidEdge.Application")
            'Get a reference to the active document
            objAssembly = objApplication.ActiveDocument
            objOcc = objAssembly.Occurrences
            Dim str As String = objOcc.Application.ActiveEnvironment
            path (0) = objOcc.Parent.FullName
            CounterObj Dim As Integer = objOcc.Count
            ReDim Preserve obj (counterObj)
            ReDim Preserve path (counterObj + 1)
            For i As Integer = 1 To counterObj Step 1
                obj (i) = objOcc.Item (i)
                path (s) = obj (i) .PartFileName

            For Each foundFile As String In path
                foundFile = foundFile & vbCrLf
                My.Computer.FileSystem.WriteAllText (
                  "C: \ temp \ test.txt", foundFile, True)

            MsgBox ("Finish")
        Catch ex As Exception
            MsgBox ("Error" & vbCrLf & ex.Message)
        End Try

    End Sub

This is my result:

D: \ Temp \ test_assembly \ Asm3.asm
D: \ Temp \ test_assembly \ cilindro.par
D: \ Temp \ test_assembly \ cubo.par
D: \ Temp \ test_assembly \ Asm1.asm
D: \ Temp \ test_assembly \ Asm2.asm


Thank you very much for the help