Cancel
Showing results for 
Search instead for 
Did you mean: 

Attempt to read or write protected memory. this is often an indication that the memory is corrupted"

Experimenter
Experimenter

Hi ,

We are trying to create an application using VC++ and WPF but when we are trying to call JTKEntityFactory::createCADExporter we are receving "Attempt to read or write protected memory. this is often an indication that the memory is corrupted" exception.

 

According to documentation it says that it is license problem. Currently we are evaluating this tool using evaluation license. Please help and let us know the steps to resolve this issue.

 

Also if we can get C# example rather then VC++ example then it would be great.

1 REPLY

Re: Attempt to read or write protected memory. this is often an indication that the memory is corrup

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Welcome to the Solid Edge Community forums. JTKEntityFactory::createCADExporter didn't ring a bell at first as any known Solid Edge API. I googled that term and found documentation for JT XT B-rep Support pdf. That is not a Solid Edge API and I'm honestly not sure where you need to go to get an answer or support.

Jason Newell
Applications Architect
www.jasonnewell.net