Batch Plot Program

Valued Contributor
Valued Contributor

Jason

 

I while back there was a batch print program posted in the solid edge bineries, that allowed you to select the printer you want and the paper size instead of using your default printer settings as the Original Batch plot did

 

With SE V18 your printer settings are saved with and when your drawings are saved. So when we print using the batch print the paper size is correct but the paper roll is what ever was last printed with.

 

Would it be hard to add the full print dialog to the batch print and have those settings over write the SE settings

 

Thanks

 

John M

 

Posted by: John Matthews
Post date: 3/16/2006 6:50:19 AM

2 REPLIES

RE: Batch Plot Program

Valued Contributor
Valued Contributor

John,

 

Do you know who wrote this batch print program that was posted in the binaries? It wasn't me so we'll need to find out who wrote it and see if we can twist their arm.

 

Posted by: Jason Newell
Post date: 3/20/2006 6:03:09 AM

RE: Batch Plot Program

Valued Contributor
Valued Contributor

It was posted br Fred Tremblay. He has modified the SE batch program to allow you to set the printer from the batch program.

 

We need to add the printer roll selection to the Batch Program. or Have the full print settings made availble through the program

 

Cheers

 

John Matthews

Hatch Engineering

 

Posted by: John Matthews
Post date: 3/20/2006 6:34:34 AM