Batch Printing using BOM for print order with report

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Looking to see if anyone has a Batch program for using the BOM to control print order.

 

Use: once printed it can be put into a binder in the same order at the BOM.

 

Also if the tool could output a log file or report of what was printed and Rev levels of what was printed. 

5 REPLIES

Re: Batch Printing using BOM for print order with report

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

I don't know of such a tool. To create one / order one you should be more accurate in your specification:

  • Under which conditions the tool shoul dbe run (i.e. from within an opened draft document and a BOM selected, or ...)
  • Should only DFTs be printed
  • How the DFTs of ASM/PAR/PSM documents could/should be found
  • Should printing be achieved in reverse order and should be printed to a single device only
  • etc, etc

 

Kind regards,
Wolfgang Kunert - www.wksyspro.de

Re: Batch Printing using BOM for print order with report

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

@jnewell has published a very good batch print tool in the past. As I never used it (I only saw the comments from satisfied users), I don't know if it still exists and/or whether it has become open source or not.

You may contact him to check, if it is possible to add your desired functionality to this tool.

Re: Batch Printing using BOM for print order with report

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Jason,

 

Are you looking for source code, or a ready made 'shrink wrapped' solution?

 

Regards,

Dave

Re: Batch Printing using BOM for print order with report

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I've talked with Jason, This is a little deeper type tool.

Re: Batch Printing using BOM for print order with report

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Would like to find a shrink wrapped version.