Cancel
Showing results for 
Search instead for 
Did you mean: 

COM object reference after model changes

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi

 

When i do some macro, i connect to Solid Edge application, then some Part Document, Model, Body and so on..

If i do some changes in the model, like Extrude ot Cut, i lose the references to the objects.

 

For example, if i do Cut, i get reference for the part, then model, face (maybe some edges). I make the Cut, then i want to use same face to do something else (maybe one more cut, or extrude). I get error, that i'm not connected to the COM object.. So i have to get reference to the part, then model, then face (there can be a lot of objects, depends on the algorhytm. Usually it takes some computing time to get all the references again, and enlarge the code..

 

There is some way to keep COM reference after model changes?

1 REPLY

Re: COM object reference after model changes

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you'll take the time to put together a small demo to reproduce the problem, I'd be happy to look at it.

Jason Newell
Applications Architect
www.jasonnewell.net