Capture entities from Broken Out View Profile

Valued Contributor
Valued Contributor

 

I have a drawing I am updating programatically. Image a rectangular box with a Broken Out Section View of the lower roght hand corner. When I change the length of the box to the point that it loses the location of the pre-existing Broken Out Section Profile, the views crap out. Since you cannot add relationships that will change with the parent geometry, I thought I could manage it programmatically.

 

Using Jason's Solid Edge Spy, if I select oone of the lines with the Broken Out Section View Profile, I can see that it is a Lines2D enitity of the Parent Sheet. However, I obviously won'y have theses entites pre-selected. That being said, where can I grab these  from? Siemens says they are not exposed and are creating a ER for it. Has anyone trun into this before?

 

Thanks!

 

Posted by: Bill Ledbetter
Post date: 10/16/2008 4:59:32 AM