Cancel
Showing results for 
Search instead for 
Did you mean: 

CheckInterference problem

Valued Contributor
Valued Contributor

 

We have written a code to check Interferences in an Assembly file. But unfortunately we are getting errors. Can somebody help us in giving us a sample code in VB or VB.NET?

Our code:

....

Dim occurrences As SolidEdgeAssembly.Occurrences

objAsmDoc.Activate()

occurrences = objAsmDoc.Occurrences

Dim set1(objAsmDoc.Occurrences.Count) As SolidEdgeAssembly.Occurrence

Dim status As SolidEdgeAssembly.InterferenceStatusConstants

Dim numInterferences AsObject = 0

Dim interferenceOccurrence AsObject = Nothing

Dim iTempCount As Int32

 

For iTempCount = 1 To occurrences.Count

set1.SetValue(occurrences.Item(iTempCount), iTempCount - 1)

Next

objAsmDoc.CheckInterference(set1.Length, set1, status, _

SolidEdgeConstants.InterferenceComparisonConstants.seInterferenceComparisonSet1vsItself, _

Missing.Value, Missing.Value, Missing.Value, Missing.Value, Missing.Value, Missing.Value, _

Missing.Value, Missing.Value, Missing.Value, Missing.Value, Missing.Value)

 

We are using .Net 2.0 and VB.NETAbove code always throws:

"The server threw an exception. (Exception from HRESULT (RPC_E_SERVERFAULT))"

 

Posted by: Siddhartha Mishra
Post date: 4/8/2008 4:30:02 AM

2 REPLIES

RE: CheckInterference problem

Valued Contributor
Valued Contributor

 

You're not going to like my answer but this is the solution.  Passing arrays from .NET to COM can be a real pain.  Often times when a method fails like this, you have to resort to using .NET reflection.Imports SolidEdgeConstantsImports System.ReflectionImports System.Runtime.InteropServicesModule Module1 Sub Main() Dim objApplication As SolidEdgeFramework.Application Dim objAssembly As SolidEdgeAssembly.AssemblyDocument Dim objOccurrences As SolidEdgeAssembly.Occurrences Dim objOccurrence As SolidEdgeAssembly.Occurrence Dim objArray As Array Dim index As Integer Dim status As SolidEdgeAssembly.InterferenceStatusConstants objApplication = Marshal.GetActiveObject("SolidEdge.Application") objAssembly = objApplication.ActiveDocument objOccurrences = objAssembly.Occurrences objArray = Array.CreateInstance(GetType(SolidEdgeAssembly.Occurrence), objOccurrences.Count) For Each objOccurrence In objOccurrences objArray.SetValue(objOccurrence, index) index = index + 1 Next Dim p As New ParameterModifier(3) p(1) = True p(2) = True Dim mods() As ParameterModifier = {p} Dim objArgs() As Object = {objArray.Length, objArray, status} GetType(SolidEdgeAssembly.AssemblyDocument).InvokeMember( _ "CheckInterference", _ BindingFlags.InvokeMethod, _ Nothing, _ objAssembly, _ objArgs, _ mods, _ Nothing, _ Nothing) 'objAssembly.CheckInterference(objArray.Length, objArray, status) Select Case objArgs(2) Case SolidEdgeAssembly.InterferenceStatusConstants.seInterferenceStatusConfirmedAndProbableInterference Console.WriteLine("seInterferenceStatusConfirmedAndProbableInterference") Case SolidEdgeAssembly.InterferenceStatusConstants.seInterferenceStatusConfirmedInterference Console.WriteLine("seInterferenceStatusConfirmedInterference") Case SolidEdgeAssembly.InterferenceStatusConstants.seInterferenceStatusIncompleteAnalysis Console.WriteLine("seInterferenceStatusIncompleteAnalysis") Case SolidEdgeAssembly.InterferenceStatusConstants.seInterferenceStatusNoInterference Console.WriteLine("seInterferenceStatusNoInterference") Case SolidEdgeAssembly.InterferenceStatusConstants.seInterferenceStatusProbableInterference Console.WriteLine("seInterferenceStatusProbableInterference") End Select End SubEnd Module

 

Posted by: Jason Newell
Post date: 4/16/2008 8:34:35 PM

RE: CheckInterference problem

Valued Contributor
Valued Contributor

 

Thanks so much for your help on this function... It's been a while I fight with it to get it works...

It's now working, but I can not get back InterferingPartsSet1 nor InterferingPartsOtherSet

 

Do you know why ?

 

thanks in advance ...

 

Anthony

 

 

 

Posted by: Anthony PONCEOT
Post date: 4/28/2008 2:15:45 AM