Cancel
Showing results for 
Search instead for 
Did you mean: 

Collapse tree in assembly

Pioneer
Pioneer

Hello there,

 

I was wondering if it is possible to collapse all items in the tree. If i want to do this right now, i  have to click all the "+"  or " -" I would like to make a macro which loops true all the items and collapse them. The shortkeys for collapse or collapse all, are not doing what i want. I want to click somewere in the assembly and then run the macro which collapses all the items.

 

I hope you guys can help me a bit with  this or tell me a way how to do it.

 

Thanks!

2 REPLIES

Re: Collapse tree in assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

Programmatically, I don't think you can do this. Interactively, you can right-click on the top node in the Pathfinder tree and select 'Collapse' from the shortcut menu to collapse everything. You can also do that for subassembly nodes to collapse everything in that subassembly.

 

Greg

Re: Collapse tree in assembly

Pioneer
Pioneer

When i do this on the top level, everything collapses and i will have to double click the top level to open it again. Of course this is an option but it takes a lot of time to do this...