Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Registry file for solid Edge addin

Experimenter
Experimenter

I have registered the plugin using "Register-SolidEdgeAddIn" in the Nuget packet manager.  

i got sucessfully registered..

 

I am creating a installer using Install shield, I have imported the .Reg file  in Install Shield. 

However I could not achieve this .. Please correct me whether i going in correct way or we have any other way to register the Addin.

 

attached my sample .Reg file

 

Please Guide me.

 

Thanks in advance.

 

 

3 REPLIES

Re: Create Registry file for solid Edge addin

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

The .reg looks good. The trick is that the CodeBase value will likely be different when it is installed on the users machine. You'll have to figure out of way in Installshield to make that value dynamic and point to the path that the addin gets installed. 

Jason Newell
Applications Architect
www.jasonnewell.net

Re: Create Registry file for solid Edge addin

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

You can use software to create setup like innosetup that allow you to register dll and create reg key


Romuald BERTIN

Re: Create Registry file for solid Edge addin

Experimenter
Experimenter

Thank you, Finally I successfully created a Addin for the Solid Edge.  I can't be acheived without you Guys.