Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating SE AddIn using VB.net Express Edition

Valued Contributor
Valued Contributor

Hello All,

 

Is it Possible to create and register an AddIn in VB.net Express Edition? I've been trying to follow the basic examples but I can't get Solid Edge to recognize/see the AddIn.

 

Any comments would be greatly appreciated.

 

Thanks!

Sergio

 

Posted by: Sergio Vallejo
Post date: 3/11/2013 7:36:24 AM

2 REPLIES

Creating SE AddIn using VB.net Express Edition

Valued Contributor
Valued Contributor

I can't say for 100% certainty but it should be possible. What version of express are you using? I've been testing [url=http://www.microsoft.com/visualstudio/eng/products/visual-studio-express-for-windows-desktop]Visual Studio Express 2012 for Windows Desktop[/url] for macros but I haven't gotten to addins yet. One of the big gotchas with .NET addins is running the correct version of regasm.exe. If you've got Solid Edge x64, you need to be running the x64 of regasm.

 

I should be working on an example soon. Everything that I'm working on these days gets published at [url=http://solidedgesamples.codeplex.com]Samples for Solid Edge[/url] so be sure and subscribe\watch for updates. We are on a monthly release cycle of the downloads.

 

Posted by: Jason Newell
Post date: 3/24/2013 11:28:56 PM

Creating SE AddIn using VB.net Express Edition

Valued Contributor
Valued Contributor

Hello,

 

yes, it's possible create and register AddIn. I maked it in Visual Studio Express 2010.

 

It's a sample AddIn in Solid Edge folder, but you must create GUID ("http://www.c-sharpcorner.com/uploadfile/anavijai/how-to-enable-create-guid-option-in-visual-studio-2... and replace GUID in "Addin.vb".

 

After that you must register (64bit):

 

c:\WINDOWS\Microsoft.NET\Framework64\v4.0.30319\regAsm /codebase d:\Your_Path\Your_AddIn.dll

 

Or unregister:

 

c:\WINDOWS\Microsoft.NET\Framework64\v4.0.30319\regAsm /u d:\Your_Path\Your_AddIn.dll

 

So worked for me.

 

Peter

 

Posted by: Peter Caderas
Post date: 8/27/2013 4:56:54 PM