Creating a text profile in a sketch

Phenom
Phenom

There are several threads about modifying a text profile, but could anyone tell me if its possible to create one.

If so, how do I do it?

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.
2 REPLIES

Re: Creating a text profile in a sketch

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you check the TextProfiles collection member, you will see that there is NO method to add a new text profile.

You can only query an existing text profile item and then change some properties of that.

Re: Creating a text profile in a sketch

Phenom
Phenom

@MartinBernhard - Thanks, I thought that might be the case.

Unfortunately there still doesn't appear to be a way to edit the text either.

We use quite a lot of engraved labels, which all have to be drawn, so I was hoping to automate the process - just key in your text on a form, click and create.

I will probably just create a template the edit size and text as required.

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.