Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom File Properties

Creator
Creator

Hello all. Please help. I've has a custom built program that has stopped working some time ago. Not sure how long maybe a year since it was last working properly. I'm running ST8 latest maintanence pack.

I'm reading a custom property from the properties of a .dft file. see line of code below

 

RsManual.Fields("PartName") = objpropertysets.Item("Custom").Item("Part Name").value

 

It appears that the Custom Property "Part Name" dose not exist, I asure you it does. Ive deleted and re entered and nope not working.

 

Has there been a change in how the property set code is written.

I have these at the top.

 

Public DB As Database
Public RsManual As Recordset
Private RS_CompiledData As Recordset
Dim ojbPdf As AcroApp
Dim objpropertysets As SolidEdgeFileProperties.PropertySets
Dim objProperties As SolidEdgeFileProperties.Properties
Dim objProperty As SolidEdgeFileProperties.Property
Dim objDoc As RevisionManager.Document

 

Thanks in advance team. really appreciate some help.

3 REPLIES

Re: Custom File Properties

Valued Contributor
Valued Contributor

Hi,

Try using Try using SolidEdgeFramework.PropertySets instead of SolidEdgeFileProperties.PropertySets so your declarations will become:

Dim objPropertySets As SolidEdgeFramework.PropertySets
Dim objProperties As SolidEdgeFramework.Properties

i've tested in SE (so not using revision manager) and this works flawlessly:

    Shared Function ReturnPartName()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDoc As SolidEdgeFramework.SolidEdgeDocument = Nothing
        Dim objPropertySets As SolidEdgeFramework.PropertySets = Nothing
        Dim objProperties As SolidEdgeFramework.Properties = Nothing

        Try
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objDoc = objApplication.ActiveDocument

            objPropertySets = objDoc.Properties
            MsgBox(objPropertySets.Item("Custom").Item("Part Name").Value)

        Catch ex As Exception
        Finally
            objApplication = Nothing
        End Try

    End Function

 

 

 

Maarten Elings | Engineer

Re: Custom File Properties

Creator
Creator

Thanks for your reply MaartenEI. Unfortunately I could not get this to run. I might add that I'm not very knowledgable when it comes to coding. I get by most of the time.

I did fail to mention that this is running inside a Microsoft Access document. I have a Custom property called "Part Name" (and many more) that I need to extract. This use to work. just not now.

 

I would like to run through revision manager as much faster, the files that I deal with are all linked up and can be up to 200 or more in the tree.

 

Thanks again

 



Re: Custom File Properties

Creator
Creator
Well.... with much digging and diving and with service pack install, everything is now going as it should. Thanks to those who helped.

Kind Regards

Nev