Cancel
Showing results for 
Search instead for 
Did you mean: 

Delete an assembly feature?

Valued Contributor
Valued Contributor

Hi,

 

In a part construction tree, we can supress an operation and we also can add a supression variable to change the status from VB.

 

How can we do the same with an assembly feature?

 

I see the assembly features, and interactively I can supress one of them, but I can't add a supression variable.

 

In the SE spy, I see the "delete" method for those features, but nothing happens calling it from VB.

 

thanks a lot

borja

 

Posted by: pepe perez
Post date: 5/22/2006 2:49:25 AM

1 REPLY

RE: Delete an assembly feature?

Valued Contributor
Valued Contributor

Hi Borja,

 

there are some problems with the API for assembly features - at least with .Net.

I have opened a PR for this - PR 1518433

 

Cheers

Calum

 

Posted by: Calum McLellan
Post date: 5/22/2006 9:48:34 PM