Cancel
Showing results for 
Search instead for 
Did you mean: 

Deleting blocks from a DFT

Valued Contributor
Valued Contributor

 

I have program that pulls blocks from a central file to build a format. Once these blaock are in the new file, I can place them on a backgroud sheet and remove them, but I cannot dlete them from the draft file. And once there in there, I cannot replace them if the one in the central file has been updated because of say the year changed.

Does anybody have any ideas?

 

Posted by: Brian Magill
Post date: 6/9/2008 4:46:30 AM

3 REPLIES 3

RE: Deleting blocks from a DFT

Valued Contributor
Valued Contributor

You have to "unblock" or "explode" them before they an be deleted. Then you need to delete the BlockOccurence from whatever specific Sheet it is used on.

 

 

Posted by: Bill Ledbetter
Post date: 6/10/2008 2:05:36 AM

RE: Deleting blocks from a DFT

Valued Contributor
Valued Contributor

 

You don't have to explode it before deleting it. Besides, I don't want anything from the block left on the sheet since I'm going to be replacing it.

The delete does remove it from the sheet but it does not remove it from the file since you are only deleting the block "occurance".

 

Posted by: Brian Magill
Post date: 6/10/2008 2:48:38 AM

RE: Deleting blocks from a DFT

Valued Contributor
Valued Contributor

I came across this recently, there is no way to delete a block from the draft file once it is in there.

I logged an IR and it was converted to a PR with number 1663220 so hopefully this will be added soon

 

Posted by: James Singleton
Post date: 6/12/2008 7:29:57 AM