Cancel
Showing results for 
Search instead for 
Did you mean: 

Determining Named Views and Configuration Names

Creator
Creator

One of the major bug bears with Solid Edge is the inability to change the orientation of drawing view once the wizard has finished.

 

I've found a way to do that using the SetViewOrientationFromNamedView method but to make it usable I really need to be able to present to a user the named views from the parent model of the view in a combobox or a list.

 

When looking at this I realised that it is also impossible to determine what configurations are available for an assembly.

 

Does anyone know how to complete these tasks?

 

I did try running the Named View Manager command but I can't see how to return the user's selection.