Cancel
Showing results for 
Search instead for 
Did you mean: 

DimStyle on Dimension gets disconnected on ST8 - MP10. Bug???

Builder
Builder

Hello there guys.

 

Not sure if this is some kind of strange bug!

 

I'm accessing Dimension.Style property, which leads to a DimStyle object, which is intended to hold specific dimension attributes ove general Style applied on a Dimension (also in other object types, like Balloon and so), as you can read from the docs.

 

The fun fact is that once I reach the DimStyle  property, saving it to a variable, it always gets "disconnected" (as I can read when debugging) after a couple of instructions. I have tried different accesing methods with the sme result. For example:

 

Dim objDimStyle As SolidEdgeFrameworkSupport.DimStyle
Dim objDimension As SolidEdgeFrameworkSupport.Dimension

...
'Code were I get dimension to work with in variable objDimension
...
objDimStyle = objDimension.Style 'DimStyle and its properties can be accessed here, as expected 'More code where I play with DimStyle properties If strKeepProperties IsNot Nothing AndAlso strKeepProperties.Count > 0 Then

'Once here, objDimStyle Properties seems to be disconnected, with no apparent reason!
...
End If

If i use Solid Edge Spy to access that property on a draft, it craches as soon as I try to read the content of DimStyle, so this seems a bug on SE. Not sure if that happens in other versions.

 

Am I doing something wrong??

 

Thanks in advanced for any help.

 

2 REPLIES

Re: DimStyle on Dimension gets disconnected on ST8 - MP10. Bug???

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I reported this issue awhile back on GitHub. See Selecting DimStyle causes ST8 crash. I didn't file an IR at the time because I wasn't sure if it was just my machine and it didn't happen in ST9. It seems like an API bug to me.

Jason Newell
Applications Architect
www.jasonnewell.net

Re: DimStyle on Dimension gets disconnected on ST8 - MP10. Bug???

Builder
Builder
Many thanks, that was really useful