Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Direction of arcs and circles

Valued Contributor
Valued Contributor

Is there a way to toggle the direction an arc is created with .net? I have noticed that mine are being created counter clockwise and I really have a need to go the other way.

 

Bob

 

Posted by: Bob Reinkemeyer
Post date: 12/2/2005 1:24:23 AM

5 REPLIES 5

RE: Direction of arcs and circles

Valued Contributor
Valued Contributor

Bob,

 

Post some code and I'll take a looksy at it .

 

Posted by: Jason Newell
Post date: 12/2/2005 2:39:58 AM

Re: RE: Direction of arcs and circles

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Jason,

 

  Here is some code.

 

Dim oApp As SolidEdgeFramework.Application = Marshal.GetActiveObject("SolidEdge.Application")
Dim oDoc As SolidEdgeDraft.DraftDocument = oApp.ActiveDocument
Dim oSheet As SolidEdgeDraft.Sheet = oDoc.ActiveSheet

Dim oArc As SolidEdgeFrameworkSupport.Arc2d
Dim xCen As Double = 0, yCen As Double = 0

'Dim xStart As Double = 0.1, yStart As Double = 0
'Dim xEnd As Double = 0, yEnd As Double = 0.1

Dim xStart As Double = 0, yStart As Double = 0.1
Dim xEnd As Double = 0.1, yEnd As Double = 0

oArc = oSheet.Arcs2d.AddByCenterStartEnd(xCen, yCen, xStart, yStart, xEnd, yEnd)

Two blocks of values are provided for the arc parameters, need to comment one and un-comment the other.

One set creates the arc and other creates its complimentary arc.

 

arc.png

What is required by both me and Bob is: creating an arc going clockwise from the start to end about the center.

The API always creates an anti-clockwise arc. This is known and accepted.

If only there is a way, trick or tweak to create a clockwise arc - this would solve many issues in several design automation processes.

 

Regards,

Tushar Suradkar

 

Re: RE: Direction of arcs and circles

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello Tushar,

you can change the Orientation property after creating the arc.

 

regards JB

regards

JB
SE 2019, VS2017

Re: RE: Direction of arcs and circles

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

JB,

 

  Thanks for the suggestion.

  Changing the Orientation property results in a complimentary arc again.

  This is same as swapping the start and end points.

  I still want the arc to go in a fashion in the image above with the given start and end points.

 

Regards,

Tushar Suradkar

 

01.png

Re: RE: Direction of arcs and circles

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

JB, I think I have been able to make use of your suggestion - it was a great suggestion, though I was not able to make use of it to solve my issue initially.

 

What I have found is for a given arc, before changing the Orientation, swap the start and end points which prevents creation of a complementary arc.

 

This results in the arc going just the other way around.

 

The original issue asked by Dylan where the solutions is used is here.

 

Thanks again.

~Tushar Suradkar

http://surfandcode.blogspot.in/

 

Does Bob Reinkemeyer who asked the original question know that a solution has been found.

Only God knows.