Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Drawing View Creation Wizard

Valued Contributor
Valued Contributor

I know the name of the drawing view that I want to add to a draft file. Is there a way to automate the task of calling the Drawing view creation wizard while skipping the task of browsing for the file. I'm using Solid Edge spy and use the start command 57082 and that brings up the browsing screen but is there a way to pass the file name to that screen. Basically I'm just trying to get rid of the browsing for a file.

 

Posted by: sean tormey
Post date: 6/16/2006 8:29:42 AM

1 REPLY

RE: Drawing View Creation Wizard

Valued Contributor
Valued Contributor

Sean,

 

There is no way that I know of the interact with Solid Edge commands like that. You'll just have to create the DrawingView manually via code.

 

Look at the DrawingViews object in the SDK. You'll want to do something like DrawingViews.Add(...).

 

 

Posted by: Jason Newell
Post date: 6/17/2006 11:45:52 AM