Edge Process is running when solidedge is closed

Valued Contributor
Valued Contributor

Hi !

 

Thanks for your helps

 

I have programmed an exe in VBnet which start SolidEdge (on the background)and do some works on the SE files and then close SolidEdge, but when the program is finished the Edge process is always running.

 

I saw through the documentation that I have to use the Olemessagefilter class. However I am not sure where I have to put the <Stathread()> because I split my program and the Solidedge files are open by a function called in the main program.

 

Have you some clue ?

 

Thanks a lot

Regards

 

Posted by: dd dd
Post date: 7/30/2012 7:26:24 AM

1 REPLY

Re: Edge Process is running when solidedge is closed

Valued Contributor
Valued Contributor

Hi myself,

 

You have to close definitely your object Application(objapplication.quit()) and document (objdocument.close()) and of course don't applied the objapplication=nothing before you quit...

 

Do I a schizophrenic ?

 

:side:

 

Posted by: dd dd
Post date: 8/1/2012 4:41:29 AM