Cancel
Showing results for 
Search instead for 
Did you mean: 

Edit HoleData not working for counterboredepth

Legend
Legend

Hello,

i want to edit existing ordered holes. Everything works fine expect the CounterboreDepth. The model is ok after editing the hole. If i measure the Counterbore, the depth is ok. But when i edit the hole feature via the dialog, it always displays the CounterboreDepth with the my standard value of 12.7 mm.

When i close the dialog with the cancel button and reopen the dialog, the correct counterboredepth is displayed!

(view in My Videos)

I tried to recompute the part, recompute the model and recompute the hole feature. Nothing works.

My sample code is attached.

Greetings from Germany
Christian Kunkel
https://c-k-m.info
1 REPLY

Re: Edit HoleData not working for counterboredepth

Legend
Legend

I found something interesting. If i set the value HeadClearance to my desired value, the parameters are correct in the dialogbox! I think the values CouterboreDepth and HeadClearance are interchanged somehow for counterboreholes.

Greetings from Germany
Christian Kunkel
https://c-k-m.info