Cancel
Showing results for 
Search instead for 
Did you mean: 

Exception when calling....

Valued Contributor
Valued Contributor

 

I have the following code snippet that gives me an exception on the line:                    

draft = (SolidEdgeDraft.DraftDocument)application.ActiveDocument;

This code loops through all *dft files and opens them one by one

Here is the sample code

            SolidEdgeDraft.DraftDocument draft = null;

            SolidEdgeDraft.Sheet sheet = null;

            SolidEdgeDraft.DrawingViews drawingViews = null;

            SolidEdgeDraft.DrawingView drawingView = null;

            SolidEdgeFramework.Variables variables = null;

            SolidEdgeFramework.variable variable = null;

            // Start exception handling

            try

            {               

                // Loop all dft files

                foreach (FileInfo fi in rgFiles)

                {                       

                    // Open current dft file;

                    application.Documents.Open(tempDir + "\\" + fi.Name, Missing.Value, Missing.Value, Missing.Value, Missing.Value, Missing.Value);

                    // Get the active document which shall be the current dft

                    draft = (SolidEdgeDraft.DraftDocument)application.ActiveDocument;

                    // Get the active document which shall be the current dft

                    sheet = (SolidEdgeDraft.Sheet)draft.ActiveSheet;                       

                    // Get all drawing views from the sheet

                    drawingViews = (SolidEdgeDraft.DrawingViews)sheet.DrawingViews;

      // code continues here.......... 

 

However if i just add the following code that waits for five seconds before opening the draft then everything works

                    // Open current dft file;

                    application.Documents.Open(tempDir + "\\" + fi.Name, Missing.Value, Missing.Value, Missing.Value, Missing.Value, Missing.Value);

                    // Wait for five seconds in order for draft document to fully open

                    Thread.Sleep(5000);

                    // Get the active document which shall be the current dft

                    draft = (SolidEdgeDraft.DraftDocument)application.ActiveDocument;

 

However I would like to avoid to have an hardcoded wait sequence (because I tried with one second first which works for most models but fails sometimes).

Is there an alternate way of doing this?

Kind Regards

 

Kjell-Åke

 

 

Posted by: Kjell-Ake Boberg
Post date: 2/10/2010 8:13:52 PM

1 REPLY

RE: Exception when calling....

Valued Contributor
Valued Contributor

Why not just set the draft object to what is returned from the open call?

 

draft = (SolidEdgeDraft.DraftDocument) application.Documents.Open(tempDir + "\\" + fi.Name, Missing.Value, Missing.Value, Missing.Value, Missing.Value, Missing.Value);

 

 

Posted by: R.D. Holland
Post date: 2/12/2010 9:42:09 AM