Cancel
Showing results for 
Search instead for 
Did you mean: 

Features Collection

Genius
Genius

is there no longer a method to rename a feature in the feature pathfinder in part?  Seems like I was once able to.

Bob Reinkemeyer
CAD Integration developer
Martin Sprocket and Gear Inc.
9 REPLIES

Re: Features Collection

Gears Phenom Gears Phenom
Gears Phenom

Sure,  RBM on the feature and select RENAME from the quick Menu or select the Feature and hit F2...

 

 

EDIT:  oops  sorry  did NOT see that htis was posted on teh Developer forum

 

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Features Collection

Gears Phenom Gears Phenom
Gears Phenom

I am able to Change the name via SE Spy...  So i have to assume it's still working. 7-14-2017 12-19-39 PM.png

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Features Collection

Genius
Genius

I saw that too.  but in the sdk it lists no method for it.2017-07-14_11-24-24.jpg

Bob Reinkemeyer
CAD Integration developer
Martin Sprocket and Gear Inc.

Re: Features Collection

Gears Phenom Gears Phenom
Gears Phenom

looks like the Name property is a member of the SolidEdgePart.SweptCutout --  not of Feature.   i assume

SolidEdgePart.SweptCutout is in the collection of Features..

7-14-2017 12-37-41 PM.png

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Features Collection

Genius
Genius

it shows up in mine under models2017-07-14_11-42-47.jpg

 

 

Bob Reinkemeyer
CAD Integration developer
Martin Sprocket and Gear Inc.

Re: Features Collection

Gears Phenom Gears Phenom
Gears Phenom

sure,  i see it in a few collections but this should provide the class structure to attempt to modify the name...

 

can you share your code up to where you are trying to set the name?

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Features Collection

Genius
Genius

oModel = oPartDoc.Models.Item(1);
oFeatures = oModel.Features;
iFeatures = oPartDoc.Models.Item(1).Features.Count;
oFeatures.Item(iFeatures).  This is where I used to be able to set it.  

Bob Reinkemeyer
CAD Integration developer
Martin Sprocket and Gear Inc.

Re: Features Collection

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

No, it won't appear since you are resolving it too far.

Make variable for each object with the right data type and it will show up.

 

Dim oFeature As SolidEdgePart.SweptCutout = oFeatures.Item(iFeatures)
oFeature.Name = "FeatureName"

Re: Features Collection

Genius
Genius

That did the trick, thanks!

Bob Reinkemeyer
CAD Integration developer
Martin Sprocket and Gear Inc.