Cancel
Showing results for 
Search instead for 
Did you mean: 

Few questions about API

Valued Contributor
Valued Contributor

Hello everyone,

 

I am researching the Solid Edge API and have a few questions.

 

1 - Is it possible to use the API to access an existing solid edge document, and grab/output the list of components?

2 - Is it possible to use the API to access an existing solid edge document, and export a particular part as identified in the parts list?

 

If you could also breifly outline, or direct me to a document that can outline how this can be done, that would be much appreciated!

 

Thankyou,

 

Mike

 

Posted by: Michael Baylis
Post date: 12/6/2011 3:50:48 PM

1 REPLY

RE: Few questions about API

Valued Contributor
Valued Contributor

Hi,

Answer 1:

You can do this in 2 ways. Opening the file and requesting the Occurrences collection.

Or via Revision Manager, you have a good example in \Custom\RevManager

 

Answer 2:

Export? What do you mean? Anyway the only way to access the part using the name shown in the pathfinder is with a function like this (for 1st level part)

 

dim oSE as SolidedgeFramework.Application = getobject(,"solidedge.application")

dim objAsm as SolidedgeAssembly.AssemblyDocument = oSE.ActiveDocument

myOcc=searchOccByName(objAsm,name)

 

From the Occurrence you can access the Document Object and whatever is inside. (Occurrence.OccurrenceDocument)

 

'---------------------

function searchOccByName(objAsm as SolidedgeAssembly.AssemblyDocument, theName as string) as SolidEdgeAssembly.Occurrence

for each occ as SolidedgeAssembly.Occurrence in objAsm.Occurrences

if occ.name=theName then

searchOccByName=occ

exit function

endif

next

end function

 

Posted by: Julian Guillo
Post date: 12/7/2011 1:30:20 AM