Form Design

Valued Contributor
Valued Contributor

After seeing the nice looking interface in Solid Edge Spy, it got me to thinking that my windows forms are plain and drab looking. Does anyone know where I can find some information on sprucing up my applications?

 

Bob Reinkemeyer

 

Posted by: Bob Reinkemeyer
Post date: 8/30/2005 8:15:43 AM

9 REPLIES

RE: Form Design

Valued Contributor
Valued Contributor

Bob,

 

www.devcomponents.com/dotnetbar

 

For $189, this is a steal . I purchased it a couple of months ago and I don't know how I made it without it. I actually did quite a bit of research before buying this product. IMHO, it's the best out there and you get more for your money than anything else that I found. This is the components that Solid Edge Spy uses for the "pretty" stuff .

 

 

 

Posted by: Jason Newell
Post date: 8/30/2005 10:08:07 AM

RE: Form Design

Valued Contributor
Valued Contributor

Got the demo version. One qestion, were do you add the code for say a menu item?

 

Bob

 

Posted by: Bob Reinkemeyer
Post date: 8/31/2005 5:23:19 AM

RE: Form Design

Valued Contributor
Valued Contributor

Bob,

 

When you installed DotNetBar, it installed a bunch of example \ demo programs that you can look at. You should be able to find them under Start -> Programs -> DotNetBar or something like that.

 

I guess I could share SES's source code with you .

 

Let me know if you still need help.

 

Jason Newell

 

Posted by: Jason Newell
Post date: 8/31/2005 6:06:46 AM

RE: Form Design

Valued Contributor
Valued Contributor

I should be able to get what I need from the sample program, thanks! I'm a little crippled in the design department. Not much natural talent here. I guess I learned function over form at the beginning. Better ugly and useful than pretty and worthless.

 

Bob

 

Posted by: Bob Reinkemeyer
Post date: 8/31/2005 6:34:40 AM

RE: Form Design

Valued Contributor
Valued Contributor

After adding a background image it seems to slow the program down to a crawl even if i'm just using like a 1x(form height) pixel that is just 1Kb or less its rather annoying. So i gave up on trying to do much with graphics, maybe someone will have some suggestions

 

Posted by: Michael Foss
Post date: 9/6/2005 6:48:24 PM

RE: Form Design

Valued Contributor
Valued Contributor

Michael,

 

What were you adding a background image to? Can you provide an example?

 

Posted by: Jason Newell
Post date: 9/7/2005 5:44:28 AM

RE: Form Design

Valued Contributor
Valued Contributor

I think VS.Net is a lot harder on system resources than VB6 was. I have 512 MB of ram, and it makes my system crawl sometimes. Get Solid Edge fired up, and it REALLY crawls.

 

Bob

 

Posted by: Bob Reinkemeyer
Post date: 9/7/2005 7:33:17 AM

RE: Form Design

Valued Contributor
Valued Contributor

http://incitetruth.com/backstrip.jpg

 

that is the image that should repeat across the background to make a nice gradiant, i'm sure for a simple gradient there is a way to do it programatically, but I only know what I've taught myself and learned from you and Bob. I figured the smaller file size should make it run faster than a bigger file. the form it is on has alot of groups that enable and disable as items are check and I think what happens is everytime things get enabled/disabled it reloads the background.

 

when I uploaded the picture it wasted to much page space so I just linked to it.

 

 

 

Posted by: Michael Foss
Post date: 9/7/2005 12:23:23 PM

RE: Form Design

Valued Contributor
Valued Contributor

Hi Michael,

 

I'm not sure why that image slows things down, but here is a small piece of code to make life easier...

 

 

Private Sub Form1_Paint(ByVal sender As Object, ByVal e As System.Windows.Forms.PaintEventArgs) _

Handles MyBase.Paint

 

'Get the graphics object from the event args.

'In another method (eg. the Load event handler) you

'can get a graphics object using

'Dim g As Graphics = Me.CreateGraphics()

'You can replace me with any control that

'has a user interface.

'Note: if you use CreateGraphics you should always

'call g.Dispose() at the end of the method.

 

Dim g As Graphics = e.Graphics

 

'Declare the rectangle to paint

Dim rect As New Rectangle(0, 0, Me.ClientSize.Width, Me.ClientSize.Height)

'Declare a gradient brush

Dim b As New Drawing.Drawing2D.LinearGradientBrush(rect, Color.White, _

Color.Blue, Drawing2D.LinearGradientMode.ForwardDiagonal)

 

'Fill the rectangle

g.FillRectangle(b, rect)

End Sub

 

Cheers

Calum

 

Posted by: Calum McLellan
Post date: 9/12/2005 7:27:32 PM