Cancel
Showing results for 
Search instead for 
Did you mean: 

Function AddderivedConfig and a query

Valued Contributor
Valued Contributor

I Have a question about following function:

 

Public Function AddDerivedConfig( _
   ByVal nConfig As Integer, _
   ByVal nZones As Integer, _
   ByVal nQueries As Integer, _
   ByRef ppsaConfigList As Variant, _
   ByRef ppsaZoneList As Variant, _
   ByRef ppsaQueryList As Variant, _
   ByVal bstrNewConfigName As String _
) As Configuration

 

I have a code wich creates a query of the class:

Solid Edge Assembly Type Library : Query Object

 

Can I use this function to create a configuration display based on this query? Or am I misinterpreting the arguments of this function?

 

Can I extract a queryList from the Query Object?

Thx for your help,

1 REPLY

Re: Function AddderivedConfig and a query

Valued Contributor
Valued Contributor

I've found a workaround to add the components of a query to a configuration.

 

The are the steps I took:

1 do a query.MatchesCount to add the components to the select set

2 use solidEdge.StartCommand to preform the show only action

3 update the configuration

 

Problem solved by alternative!