Get PhysicalProperties without opening Part/Assembly

Valued Contributor
Valued Contributor

I'm using the "ReportBOM" assembly Sample to create a small tool which copies all the basic info from a assembly (and all of its sub-assemblies and parts) to Excel.

 

In this Sample the information is gathered using SolidEdgeAssembly.Occurrences, and using it I can read all data I want except for the PhysicalProperties (I mainly need the Mass of each component/ass'y)

Is there a way to get the mass of a assembly part(/sub assy) without opening it?

 

Maarten Elings | Mechanical Engineer
1 REPLY

Re: Get PhysicalProperties without opening Part/Assembly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello MaartenEl,

you can use the OccurrencesDocument property of the Occurrence object to acces the Part/Subassembly from the open assembly.

 

There is no other way to get the physical properties of these documents.

 

When you get an instance of a OccurrenceDocument, then the Occurrence ist activated, what means that the document is loaded to memory (open).

 

Regards Jürgen

regards

JB
SE ST10