Cancel
Showing results for 
Search instead for 
Did you mean: 

Get Plane as NURBS surface

Creator
Creator

Hey guys,

 

I asked a question in the SolidEdge Forum and was pointed on this developer forum because it might fit the question better. Please take any information from the existing thread: http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Get-Plane-as-NURBS-surface/m-p/30737...

 

If there are further questions about the problem, please don't hesitate to ask. Smiley Happy

 

Thanks in advance

Marcel

2 REPLIES

Re: Get Plane as NURBS surface

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

AFAIK, there are no direct methods in the API to convert any geometry into a NURB surface.

You can, of course, query the specific parameters for each type of geometry, like the origin and the normal of the plane, but the conversion has to be done by you.

I think OpenCASCADE is an Open Source project with an SDK function to convert any geometry to NURBS, except planes ;-)

Re: Get Plane as NURBS surface

Creator
Creator

That's what I suspected. Thank you very much for the information.