Get model coordinates of pattern elements

Creator
Creator

Hi All,

 

I'm finding it difficult to get the model coordinates of center points of holes created using circular pattern feature. It will be really helpful to me if anyone could suggest a solution for this issue

 

Solid Edge ST9

VB.NET

 

With Regards

Admin2

2 REPLIES

Re: Get model coordinates of pattern elements

I do not see a way to get an X|Y matrix.

 

You would need to interogate the pattern type and inputs and do the math yourself...

 

But maybe using the Draft's Hole Table might be a solution.

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6

Re: Get model coordinates of pattern elements

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi @Admin2,

@MattJohnson_PG is right. In principle there are no point cooridinates for a hole pattern exept the 2D Profile of the pattern definition.

The holes only have center axis that you could intersect with some plane to get points...

regards

JB
SE ST10