Cancel
Showing results for 
Search instead for 
Did you mean: 

GetEllipseCount

Valued Contributor
Valued Contributor

Using SE V19 and Visual Basic 6.0 or .Net 2003. I have an open draft file. I need to know if the file has any ellipses on it. I thought the GetEllipseCount method would work but I have gotten no success with it. The syntax is supposed to be Object.GetEllipseCount but I can't figure out what the object is. I have tried the draft file, the sheet, the drawing view, all with no luck. It errors out. Has anybody else tried to use this method?

 

 

 

Posted by: sean tormey
Post date: 12/4/2006 6:20:58 AM

1 REPLY 1

RE: GetEllipseCount

Valued Contributor
Valued Contributor

Sean,

 

I'm not sure this is what you're looking for because the GetEllipseCount() method is a member of DisplayData which can be found here:

 

SolidEdgeFrameworkSupport.DisplayData.GetEllipseCount()

 

Application.DraftDocument.Sheets.Sheet.Dimensions.Dimension.DisplayData

 

HTH

 

Posted by: Jason Newell
Post date: 12/4/2006 6:28:29 AM