Cancel
Showing results for 
Search instead for 
Did you mean: 

Getting File Properties without SE installed

Valued Contributor
Valued Contributor

I can't remeber exactly how I did this previously, but maybe someone has an idea.

I need to run a program that reads and sets the SE Properties without the file open. The program already exists and runs fine. How do I get this to run on a machine that does not have Solid Edge installed?

 

It looks like I copied PropAuto.dll, jdocres.drx, and PropMgr.drx for v19. However, I can't get the program to work on a new machine with ST4 (64bit) dlls and drx files. Is there a specific location they need to be? Do I need to register anything? I just don't remember how I did it before.

 

Or is there an easier method?

 

Thanks.

Carl Breving

 

Posted by: Carl Breving
Post date: 10/23/2012 8:11:55 PM

1 REPLY

Getting File Properties without SE installed

Valued Contributor
Valued Contributor

I figured out the dlls I was missing using dependency walker. But does anyone know of an easier way to use the File Properties API without installing these dlls?

 

Posted by: Carl Breving
Post date: 10/23/2012 9:39:42 PM