Cancel
Showing results for 
Search instead for 
Did you mean: 

Getting the Parlist height setting

Creator
Creator

For a tool we are developping (with ST7), we want to:

  1. Get the height of the Partlist on the drawing
  2. Change the style (Saved settings) of the Partlist (this resets the height)
  3. Set the height recorded at step 1.

We can get and set the height of a Partlist with the SolidEdgeDraft.Parlist object using these properties:

  • MaximumRows
  • MaximumRowsFirstPage
  • MaximumRowsAdditionalPages
  • MaximumHeight
  • MaximumHeightFirstPage
  • MaximumHeightAdditionalPages

 

The issue we have is that doing it also changes the Height setting from "Maximum number of data row" to "Maximum height":Capture.PNG

Since these two are not necessarily equivalent, is there a way to get/set the value of the Height setting via the SDK? Or is there a way to bypass the issue?

 

Thanks a lot.

 

 

 

3 REPLIES

Re: Getting the Parlist height setting

Valued Contributor
Valued Contributor

Hi,

 

Please refer below links for Table style detials.

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Developer-Forum/Change-colors-of-table-li...

 

http://support.industrysoftware.automation.siemens.com/training/se/107/api/SolidEdgeFrameworkSupport...

 

since in ST6, we dont have option for tablestyles "SolidEdgeFrameworkSupport.TableStyles".

 

i am not able to give you specific answer for you.

 

but if you use solidedge spy, you will get more details about "partlist details"

 

Capture.PNG

 

Thanks,

Bala.

Re: Getting the Parlist height setting

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi dosti,

the table maximumxx properties are not part of the table styles, they are properties of the PartList object.

If I undestand you right, you are searching for a way to read if per height or per rows options is selected.

Reading the properties will give you the values of both and will change nothing in the table.

Writing the properties will change to either per rows or per height depending on the last written value.

 

I did not find a method to read the current mode, sorry.

You should create an IR for this (GTAC)

regards

JB
SE ST10

Re: Getting the Parlist height setting

Creator
Creator

Thanks JB, yes I'm trying to read the current mode. I'll fill an ER as suggested.