Cancel
Showing results for 
Search instead for 
Did you mean: 

Grabbing variables from Adjustable Parts

Valued Contributor
Valued Contributor

 

I'm trying to find exposure to the Variables in an Assembly which relate to the variables from an Adjustable Part.

For example, lets say I have a piece of Tubing that is modeled in the native part at 48" long. When I bring it into the Assembly, because it is an Adjustable Part, I set the length to 60". I can't find exposure to that variable anywhere.

Does anyone have any thoughts on how to capture that value for use in say a Parts List?

 

Thanks!

 

Posted by: Bill Ledbetter
Post date: 10/31/2008 4:28:26 AM

1 REPLY 1

RE: Grabbing variables from Adjustable Parts

Valued Contributor
Valued Contributor

I've found what I think exposes the info - but I can't get the info from the API.

 

seDOC..Occurrences.Item(1).AdjustableDefinition.GetAdjustables(NumberOfEntries, PartVariables, AsmVariables)

 

Can anyone give me an example which would make the above API spit out the info? I've tried so many different approaches and can't get it to work properly.

 

Thanks in advance,

 

 

Posted by: Bill Ledbetter
Post date: 11/3/2008 12:41:01 AM