Cancel
Showing results for 
Search instead for 
Did you mean: 

HELP! Need simple batch MACRO for SE

Creator
Creator

Hi there,

 

I am trying to create a batch macro that takes several individual .dft documents (only one sheet inside) and combines them into one only document (with many sheets). I dont mind if the macro copies/pastes the whole sheet, or only the content in the sheet into a new sheet. 

 

I have been searching the internet, but found very little information, and did not manage to do it myself. 

 

For this reason, I would like to ask if anybody could help me do it. I am even willing to pay a reasonable price for the job. 

 

Thank you very much in advance,

Jose Mora 

 

6 REPLIES 6

Re: HELP! Need simple batch MACRO for SE

Creator
Creator

Somebody..? 

Re: HELP! Need simple batch MACRO for SE

Siemens Phenom Siemens Phenom
Siemens Phenom

@Tushar would this be something for you?

Re: HELP! Need simple batch MACRO for SE

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor
I remember doing a reverse of this recently where sheets from a single DFT file were required to be written out as separate DFT files.
In that case the file was simply saved as and 'all but one' sheet was deleted.

I will take the copy-paste hint and explore the possibility of any helpful API.

Please give me time till this weekend to check feasibility.

Tushar
www.SurfAndCode.IN
www.CADVertex.com

Re: HELP! Need simple batch MACRO for SE

Creator
Creator

Dear All, 

 

First of all, thank you all for your kind help. 

 

I try to explain as best as possible. 

 

We start with a list of .dft documents, each of them with one single sheet inside, containing a 2D drawing. 

We would need the macro to:

     - Create a new .dft (or open a blank .dft template)

     - Open the first .dft document in the list and copy/paste the whole sheet in the new .dft.

     - Repeat in batch mode through the rest of the list. 

 

IMPORTANT INFO

-->  The number of .dft docs in the list is not fixed. It will vary, so the Macro will have to count them, or have an input variable (number of docs), which will be introduced manually before running the macro. 

-->  If possible, we would prefer giving the input .dft list as follows: 

 

.dft MACRO.PNG

Solidedge version used: ST6

 

 

Looking forward to hearing your thoughts!!

 

Re: HELP! Need simple batch MACRO for SE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi all,

 

Last time a customer ask for this sort of fonctionallity we ended saving multiple documents as PDF then make a fusion of those PDF.

Creating draft document with a big number of sheets isn't a good idea for save and update.

 

In case you really need to add all the sheets to a document here is an example where we add all the sheets for the documents in the folder training of Solid Edge 2019 in an open draft file.

 

    Private Sub Start_DraftFusion()
        Dim objApp As SolidEdgeFramework.Application = Nothing
        Dim objDoc As SolidEdgeDraft.DraftDocument = Nothing

        Dim FileList As New List(Of String)

        FileList.AddRange(System.IO.Directory.GetFiles("C:\Program Files\Siemens\Solid Edge 2019\Training", "*dft"))

        Try
            objApp = SolidEdgeCommunity.SolidEdgeUtils.Connect()
        Catch ex As Exception
            objApp = Nothing
        End Try

        If objApp IsNot Nothing Then
            'Get Draft Document
            Try
                objDoc = DirectCast(objApp.ActiveDocument, SolidEdgeDraft.DraftDocument)
            Catch ex As Exception
                objDoc = Nothing
            End Try
            If objDoc IsNot Nothing Then
                Dim SheetList As New List(Of String)
                For Each objsheet As SolidEdgeDraft.Sheet In objDoc.Sections.WorkingSection.Sheets
                    SheetList.Add(objsheet.Name)
                Next
                For Each myFile In FileList
                    CopySheet(objDoc, SheetList, myFile)
                Next
            End If
        End If

    End Sub
    Private Sub CopySheet(ByRef TargetDoc As SolidEdgeDraft.DraftDocument, ByRef TargetSheetList As List(Of String), ByVal FileName As String)
        If File.Exists(FileName) Then
            Dim SourceDoc As SolidEdgeFramework.SolidEdgeDocument = Nothing
            Try
                SourceDoc = TargetDoc.Application.Documents.Open(FileName)
            Catch ex As Exception

            End Try
            If SourceDoc IsNot Nothing Then
                For Each objsheet As SolidEdgeDraft.Sheet In SourceDoc.Sections.WorkingSection.Sheets
                    'Get BackGround name
                    Dim SourceBackGroundSheet As String = ""
                    Try
                        SourceBackGroundSheet = objsheet.Background.Name
                    Catch ex As Exception

                    End Try
                    SourceDoc.Activate()
                    objsheet.Activate()

                    'Copy Data
                    Dim objSelectSet As SolidEdgeFramework.SelectSet
                    TargetDoc.Application.ActiveSelectSet.RemoveAll()

                    objSelectSet = TargetDoc.Application.ActiveSelectSet
                    objSelectSet.SuspendDisplay()
                    objSelectSet.AddAll()
                    objSelectSet.Copy()

                    Dim NewSheetName As String = objsheet.Name
                    If TargetSheetList.Contains(NewSheetName) Then
                        Dim i As Integer = 1
                        Dim NewSheetNameCompute As String = NewSheetName
                        Do While TargetSheetList.Contains(NewSheetNameCompute)
                            NewSheetNameCompute = NewSheetName & "_" & i
                            i += 1
                        Loop
                        NewSheetName = NewSheetNameCompute
                    End If

                    'Create New Sheet
                    TargetDoc.Activate()
                    Dim ObjNewSheet As Sheet = Nothing
                    Try
                        ObjNewSheet = TargetDoc.Sheets.AddSheet(NewSheetName, SolidEdgeDraft.SheetSectionTypeConstants.igWorkingSection)
                    Catch ex As Exception

                    End Try
                    If ObjNewSheet IsNot Nothing Then
                        ObjNewSheet.SheetSetup.SheetSizeOption = objsheet.SheetSetup.SheetSizeOption
                        For Each objBackGround As SolidEdgeDraft.Sheet In TargetDoc.Sections.BackgroundSection.Sheets
                            'Get BackGround Infos
                            Try
                                If objBackGround.Name = SourceBackGroundSheet Then
                                    ObjNewSheet.Background = objBackGround
                                    Exit For
                                End If
                            Catch ex As Exception

                            End Try
                        Next
                        ObjNewSheet.Activate()
                        TargetDoc.Application.DoIdle()

                        'Paste in New Sheet
                        TargetDoc.Application.ActiveWindow.Paste()
                        TargetDoc.Application.DoIdle()

                        TargetSheetList.Add(NewSheetName)
                        objSelectSet = Nothing
                    End If
                Next

                SourceDoc.Close(False)
            End If
        End If

    End Sub

Note that this is only an example and may need some adjustment and debug, for example I'm not sure if background sheet are correctly handle.

 

 

Regards,

Romuald

Re: HELP! Need simple batch MACRO for SE

Creator
Creator
Thank you very very much Romuald.

I will try to adjust and make it work Smiley Wink

BR,
JM